11/27/2008 9:57 PM | |
Joined: 12/27/2007 Last visit: 8/21/2022 Posts: 12 Rating: (0) |
i want to read one word or bool from the Simotion D425 using OPC beetween my PC and SIMOTION. but i have problem.I have attached to picture. it explain my problem . please can you check it. Have a nice day. Attachmentopc.zip (372 Downloads) |
1/8/2009 1:21 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985)
|
Hello, look at the pdf in attachment. The documented way works fine. The error occurs when the symbolic file ist not configured correctly. Regards Christoph AttachmentProductinformation_SIMATIC_NET.pdf (364 Downloads) |
1/18/2009 11:48 PM | |
Posts: 7 Rating: (0) |
I saw the same using. The exported files from the simotion is being placed in the wrong place on the computer for use with the opc. see attached. BRALST AttachmentPages from Productinformation_SIMATIC_NET.pdf (287 Downloads) |
1/18/2009 11:49 PM | |
Posts: 7 Rating: (0) |
see attached correction to the opc manual. BRALST AttachmentPages from Productinformation_SIMATIC_NET.pdf (349 Downloads) |
Follow us on