10/21/2020 6:13 PM | |
Joined: 6/9/2020 Last visit: 12/24/2020 Posts: 5 Rating: (0) |
Hello, everybody, I am using MCD-SIMIT-TIA-SIM ADVANCE for digitalization. but i have a problem with bus synchronous with TIA. what can i do for this? I am getting this error when ı start the system asynchronous mode. so this mode is not usefull. because i need to synchronous system. [snip] ı am getting this error because MCD is opennig faster from SIMADVANCE and MCD is want to connect with SIM ADVANCE but SIMIT is not open the SIM ADVANCE yet. But when i start the bus synchronous mode i am getting this problem: [snip] I need to start my system with bus synchronous mode for true simulation to my system. So how can ı solve the second pictures problem?? Applications versions which i use: TIA Portal V15.1 PLCSIM Advanced V2.0 SP1 SIMIT 10.1 NX MCD 1872 ------------------------------------------------------------------------------------------ Attachmentimages.zip (711 Downloads) |
Last edited by: Jen_Moderator at: 10/22/2020 09:02:44New subject after splitting Last edited by: Ozcan Ozaltin at: 10/22/2020 09:37:50Edit Last edited by: Ozcan Ozaltin at: 10/22/2020 10:00:32Last edited by: Jen_Moderator at: 10/26/2020 10:13:16Removed links and added files as an attachment. Güven Mühendislik Makina |
|
Follow us on