4/2/2014 7:53 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Dear NADIM Please Check the following : 1) Re-check the parameters set by you P081= 1 - Field Weakening Activated: For this settingField Weakening Optimisation must be executed P083=4 - Actual Speed Feedback - Freely Wired ? P100=1 - Rated Armature Current = 1 Amp P102=0.01 - Rated Field Current = 10ma !!!!! - Tthe Parameters set by you are for DC Motor with Field Wekening. For Bulb Load , you should set as follows : P081 = 0 : No Field Weakening P082 = 0 : Disable Field P083 = 3 :Actual Speed Feedback = EMF Actual Value 2) Do you have the Safety Shutdown contact wired across XS : 105 - 106 ? 3) What is the Operating Status r000 indicated on the drive. This will indicate whether the Drive is waiting for any pre-conditions for Run. a) Pl Download the 6RA70 Manual and read Ch 6 & 7 for wiring and Startuo b) Pldownload and use Drivemonitor software from the link and use the same for commissioning. Drivemonitor also includes an "Assisted Commissioning" wizard to easily startup and run a drive. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 4/2/2014 9:53 AM: Last edited by: Navnag at: 4/2/2014 7:53 AMThere is no such thing as the last bug in a program |
|
4/4/2014 8:38 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello NADIM For this, you should simply use a adjustable DC power supply. That will be much simpler and easier than using a 6RA70 for the task. We have a saying ... why use a sword, where only a needle is needed to do the job Cheers Navnag |
There is no such thing as the last bug in a program |
|
4/4/2014 11:05 AM | |
Posts: 5 Rating: (0) |
Dear Sir, Thanks for your suggestion. But this customer requirement not mine. I am still waiting for a reply. Regards, Nadim
|
4/4/2014 1:42 PM | |
Posts: 5 Rating: (0) |
Dear KSN If you cant help then no need to bother. I am just requesting for help.
|