5/16/2012 4:47 PM | |
Joined: 4/19/2008 Last visit: 5/28/2024 Posts: 1525 Rating: (159) |
Hello sureking, Yes open the Hardware Configuration, Select your S7-300 CPU, Click the Download Button, then you will see Accesible Node Window Select the PLC by Clicking the Search button, then Download..... then Try to Download the OB1... Have a look on the Demo..... Testing and Commissioning Functions Demonstration System: SIMATIC Webcast Tutorials |
Ammy |
|
This contribution was helpful to1 thankful Users |
5/16/2012 7:14 PM | |
Posts: 14 Rating: (0) |
Ammy, I tried according to your instructions and my best knowledge. I couldn't go further. Please help me check the pictures I took and give me some suggestions. Thanks. |
5/16/2012 7:15 PM | |
Posts: 14 Rating: (0) |
Picture 2. |
5/16/2012 8:09 PM | |
Posts: 14 Rating: (0) |
pic 2 |
5/17/2012 2:34 PM | |
Posts: 14 Rating: (0) |
Ammy, If I click on view, it will get into a forever waiting state. By "forever", I mean I waited soooooo long and no response. Then I terminated it. |
5/17/2012 4:02 PM | |
Posts: 691 Rating: (36) |
Is it that you you are trying to download in MPI , but your CPU MPI Port is configured in DP? Can you send us the Pics of PLCSIM and CPU Configured? |
5/17/2012 4:37 PM | |
Posts: 559 Rating: (87) |
Dear sureking, When you are starting PLCSim, Please check that PG/PC interface didn't automatically change to the appropriate one (PLCSIM MPI in Your case). If yes then change it manually and also try with different project and MPI, and after this it should started to work normally. Also refer to below Post which has same problem as you /tf/WW/en/Posts/73323 Best.. |
5/17/2012 4:58 PM | |
Posts: 14 Rating: (0) |
I have already done that. I had checked that link before I posted my question. |
Follow us on