4/20/2012 9:03 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
I guess that application is working. So, there should be configured some data to be exchange between CPU and MM4. Take a look at For MICROMASTER 4 and for SINAMICS G120/G120D frequency inverters, which parameters can be read-out using PZD? That FAQ can give a starting point in order to undesrstand what have already been configured there and then with small changes to get the wished signals. Best regards, Hristo Mihalev
|
Last edited by: UMENCHO at: 4/20/2012 9:04 PM |
|
4/27/2012 3:53 AM | |
Joined: 9/27/2006 Last visit: 5/21/2024 Posts: 12257 Rating: (2668) |
Hello BRhyno; To give you a more informed answer to your question, may I suggest this document: Operating Instructions: MICROMASTER PROFIBUS Optional Board A more compact version of this information can be found here: Which terminology do you use for cyclic PROFIdrive communication? In the first section you will be presented with the Profidrive Profile Objects PPO1 to PPO5, whichdeterminediffferent size PKW and PZD in the Profibus telegram. You select which PPOx you will use in theHWConfig editor, when you select the exchange parameters of the drive as a Profibus slave. Using the PKW mechanism you can read and write any parameter you wish inside the drive, but you can do it only one parameter at a time, anm you must program the read/write operation as explained in the section "PKW mechanisms for parameter processing" of the manual above. See also the following FAQ: How do I read / write parameters using PROFIBUS on the MICROMASTER 4 and CU240S/D DP/DP-F and PROFINET on the CU240S/D PN/PN-F? On the other hand, selecting PPO2, PPO4or PPO5 will give you 6 or 10 PZD words that can be associted with (respectively) 4 or 8 parameters in the cyclic exchange of data, so you can monitor these as required (the Control word and the Speed reference are 2 PZD values that cannot be changed in the PZD transmission). This FAQ will discuss how parameters of the drive can be read out through the PZD mechanism. For MICROMASTER 4 and for SINAMICS G120/G120D frequency inverters, which parameters can be read-out using PZD? You will find different program samples explaining the different mechanisms of Profibus-DP exchanges in the following link: Are there program examples for the Instruction Manual of the MICROMASTER PROFIBUS option module? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/27/2012 3:59 AMBegging Umencho''''s forgiveness, I just reread his earlier post and noticed that the links he already proposed are also used in my post. Redundant info, sorry. |
|
This contribution was helpful to1 thankful Users |
4/27/2012 7:37 PM | |
Posts: 1064 Rating: (72) |
Take a look at this it might help you http://support.automation.siemens.com/WW/view/en/8894584 |
7/27/2015 12:04 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
Follow us on