12/25/2019 8:03 AM | |
Joined: 12/22/2017 Last visit: 1/12/2021 Posts: 2 Rating: (0) |
I am also following the same issue i ca control the the drive speed by CTRL_PTO but i cannot use Technology functions.MC_HOME kind of.. how to synchronize the PTO to technolgy objects ------------------------------------------------------------------------------------------ |
Last edited by: Sani12345 at: 12/25/2019 08:03:45Last edited by: Jen_Moderator at: 12/25/2019 13:43:22New subject after splitting |
|
12/26/2019 6:49 AM | |
Joined: 10/24/2012 Last visit: 6/1/2024 Posts: 310 Rating: (21) |
You can use one function at a time i.e either you can use CTRL_PTO or the SIEMENS built in technology blocks which are MC_power for enabling the technology object then MC_Home or MC_relative motion etc. you are using the CTRL_PO block by activating the PTO from the hardware configuration.If you want to use MC_Home, MC_velocity block etc then you have to add technology object and don't activate the pulse generator from the hardware configuration. Please see the attached file for complete understanding. https://support.industry.siemens.com/cs/attachments/109741731/s71200_motion_control_function_manual_en-US_en-US.pdf?download=true Regards, |
Kashir Saeed. |
|
Follow us on