11/10/2021 7:06 AM | |
Posts: 2 Rating: (0) |
Hi, I have a problem with micro master 440, I am not able to control the speed from scada(starting and stopping is ok) , I checked 4-20mA ok, please let me know any solution, is there any parameters to control the speed ? There is one more drive if I give 25% speed reference the drive running with 75 % speed, if I give 0% drive running at 100% ( command is reversing) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/10/2021 13:16:44New subject after splitting |
|