1/13/2017 6:09 AM | |
Posts: 1 Rating: (0) |
Hello everyone, Is there a patch that works on windows 10 for the same issue? Thanks |
Last edited by: sagemlink at: 1/13/2017 6:09:55 AM |
|
4/24/2017 4:36 PM | |
Posts: 1 Rating: (0) |
Hello If one driver to send my friends. Driver for PC/PPI cable 6ES7 901-3CB30-0XA0Thank you
|
11/29/2017 9:59 PM | |
Posts: 439 Rating: (108) |
Hello, Thanks luciferC4, your patch solve an issue one of my customer had. He installed "STEP 7-Micro/WIN V4.0 SP6" which is not compatible with Windows 7. At this point he was not even able to uninstall "STEP 7-Micro/WIN V4.0 SP6" or to install/upgrade "STEP 7-Micro/WIN V4.0 SP9" (which is compatible with Windows 7) First thing: (This is what I found first, but did not solve all the issue) How do you uninstall STEP 7 Micro/WIN V4.0 after an aborted installation? Second thing: (This is what USA tech support gave me)
He was able to install "STEP 7-Micro/WIN V4.0 SP9" at this point. Then, he had issue with the Set PG/PC interface. He was not able to select "Micro/Win" in the "Access Point of the Application" list. I runned you .BAT file and it solved everything. Here is the contain of it:
Create a text file, copy/paste the above command in it and change the .txt to .bat and run it as administrator. I am now able to select "PC/PPI.cable.PPI.1" and also "Micro/Win". Thanks! Best regards, Hugo |
Last edited by: Jen_Moderator at: 11/30/2017 1:50:49 PMAdded picture as an attachment. |
|
This contribution was helpful to2 thankful Users |
3/25/2018 4:38 PM | |
Posts: 3 Rating: (0) |
Yes working good. Thanks you save,from lot of troubles |
4/19/2018 12:59 PM | |
Posts: 1 Rating: (0) |
Hi This patch works, I had been struggling for days with this problem and this patch solved my access issue. thanks for posting this kind regard Andy |