6/24/2013 6:51 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836)
|
Hello, Please tell us values of P2000.
|
Ayman Elotaify |
|
6/24/2013 6:58 PM | |
Posts: 97 Rating: (3) |
hi P 2000 is also set to 88.0Hz |
Last edited by: KonradR at: 6/24/2013 7:07 PM |
|
6/24/2013 7:16 PM | |
Posts: 97 Rating: (3) |
hi, (want)speed 22Hz at 1.4v. actual speed 12Hz at 1.4v P1080 - 0.0 P1082-88.0 P2000-88.0 regards Konrad |
6/24/2013 7:31 PM | |
Posts: 97 Rating: (3) |
hi do you recomend to set P2000 at 160Hz what will give 22.4Hz at 1.4V . regards Konrad |
6/24/2013 9:35 PM | |
Posts: 97 Rating: (3) |
hi all, i have some more data at 0.4v to be at 4.4Hz 0.7v to be 19Hz 1.4v to be 22Hz 2.5v to be 25Hz 3.2v to be 28Hz 6.9v to be 53Hz regards Konrad |
6/24/2013 9:41 PM | |
Posts: 97 Rating: (3) |
Vithani After puting your settings the drive went to its maximum speed straight away. regards Konrad |
6/24/2013 11:04 PM | |
Posts: 97 Rating: (3) |
if its about source input is given from siemens s5 output card |
Follow us on