7/24/2020 12:42 AM | |
Joined: 12/23/2008 Last visit: 4/19/2024 Posts: 29 Rating: (6) |
Did someone managed to solve this issue without changing config at the PLC? We have some Factory Link apps running being migrated over WinCC, and the perfomance of the tags update in the Factory Link are way better then the WinCC Driver. I believe it has something to do with the differents DataSet handling over the Factory Link application. What we did to improve a little bit the speed was to split the connection in 4 (same IP and ports) to split the tag number over them. That made it faster but not as fast as Factory Link. Anyone has any other hints?? Regards!! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/24/2020 06:46:52New subject after splitting |
|