10/10/2019 10:50 AM | |
Posts: 14 Rating: (0) |
and here attachme another two clips, i donlt know why we can not upload 3 or more pictures in one topic. who knows? |
10/10/2019 10:52 AM | |
Posts: 14 Rating: (0) |
picture -3 for the download problem.
|
10/10/2019 11:11 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi hankbiao, Simatic-H-Station are not supported by PLC-Sim. this is mentioned in the help of PLCSim, and also in this FAQ: What is the difference between S7-PLCSIM and a "real" automation system? hope this helps, regards, |
Last edited by: mopS04 at: 10/10/2019 11:12:44Last edited by: mopS04 at: 10/10/2019 11:13:25Last edited by: mopS04 at: 10/10/2019 11:15:11FCK WAR! |
|
10/11/2019 7:38 AM | |
Posts: 14 Rating: (0) |
hi, mops04, i am not do the plcsim testing in my real station, i just want to try to test PLC logic program by VMware workstaion using my own individual laptop, so i have to operate PLCSIM, and download the program to the virtual machine (VIRTUAL CPU , can be called) best regards.
|
11/26/2020 2:17 PM | |
Joined: 6/9/2020 Last visit: 11/22/2023 Posts: 2 Rating: (0) |
Hi, I had the same problem and I solved by remove and re-install the PLCSIM |