4/24/2012 10:35 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
I'm not sure but I think eMail notifications is only used to inform you whenever a topic you subscribed on, is updated. Not when you received a PM. Brgds. |
B r g d s , |
|
4/24/2012 11:11 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
Dear Users, at the moment, there is no notification when new private messages arrive. Moderators got private messages each day. So when the counter of messages changes from 0 to 1 normally we realized this very fast. There are thoughts about an configurable email notification for all those which are not so often online. Let's wait and see what could be done The idea with something like a popup is interesting. Maybe not only for private messages? We will have a thought about it after the campaign. So thank you for all your ideas to make this grandiose platform even better Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to2 thankful Users |
4/24/2012 11:28 AM | |
Posts: 133 Rating: (9) |
That would be an awesome feature because to be honest I dont even look at my Private messages. |
This contribution was helpful to1 thankful Users |
4/25/2012 9:59 AM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
Keep in mind that often browser have build-in popup blockers that some people don't even know about. Perhaps it's possible to change the color of [color=red]Private Messages (5)[/color] and put it in bold if there are any? |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
7/17/2013 5:33 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
Hello there. I made a script for GreaseMonkey Addon (I'm using Mozilla Firefox) that will send you a popup window whether the number in a link Private Messages (0) is greater than zero. It works only on Forum pages. The "Private Messages" page is excluded — no popups here. The basic part of the script: [code]var links = document.getElementsByClassName('arrow'); var lnkLength = links.length; var msgObj = null; var msgAmount = 0; for ( var i = 1; i < lnkLength; i++ ) { if ( links[i].text.search("Private Messages ") == 0 ) { msgObj = links[i]; break; } } if ( msgObj != null ) { msgAmount = msgObj.text.match(/\d+/); if ( msgAmount > 0 ) { alert('You have ' + msgAmount + ' unread private messages!'); } }[/code] My script is registered here: http://userscripts.org/scripts/show/173535 For the comments, ideas, usage, upgrades — Thank You. This is my second GM script after the floating Forum's top field. |