5/15/2018 11:37 AM | |
Joined: 2/14/2012 Last visit: 7/10/2023 Posts: 88 Rating: (21) |
Hi all, This is a follow up question from the thread graphically write protected in symbol script editor. We have a number of base object symbols that have the wrong specification called in the symbol script. I just built a base object query to search for all the symbols with the wrong specification (which is a big help already). Now is there a way to replace a textstring within the symbol script? I tried with the VB command "replace" but it did.t work: replace a.DevSymbols.Item("M40_P2").OwnScript, searchstring, replacestring many thanks Th. |
5/16/2018 8:17 AM | |
Joined: 2/14/2012 Last visit: 7/10/2023 Posts: 88 Rating: (21) |
Hallo Jiri Thanks a lot for your help. Works great. This will save us a lot of time. Greetings ¨Th. |