9/10/2012 11:42 AM | |
Posts: 99 Rating: (0) |
Dear Mike, please see the below details regarding the problem, Operating System detail & SW, - Windows 7 ultimate 32 bit - SICAM PAS PQS V3 - SIMATIC IPC DIAG MONITOR V4.3 - SIMATIC NET. SOFTNET IE RNA Problem #1: SNMP Devise in the UI Operating is showing only the connected SWITCHES, Time Server. For HMI, Full Server & Gate Way, they are always in the standby mode although, 1- We can ping from full server 1 to 2 and vise verse. 2- We can access remotely from full server 1 to 2 and vise verse. - For number two we can only make it when the client for Microsoft NW option is: selected. Note: RUGGEDCOM SWITCHES can’t be access from Full Server, HMI and Gate Way. For this problem we did the following; We add “TLS_RSA_WITH_DES_CBC_SHA” registry key in the below path; “HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Cryptography\Configuration\Local\SSL\00010002” Dose the added registry key affect our SICAM PAS? can you please advise if there is any hotfix we need to put in the system thanks AttachmentVisio-SICAM PAS.pdf (144 Downloads) |