7/1/2013 6:41 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359)
|
Hello, What kind of network ?PROFIBUS,ETHERNET or MODBUS? For 2 first cases, check the "s7 connection" between each selected partner. see the sample for 2 partners: How do you simulate communication between two CPU modules? Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 7/1/2013 6:49 AM |
|
This contribution was helpful to3 thankful Users |
7/1/2013 6:50 AM | |
Joined: 5/28/2008 Last visit: 5/26/2024 Posts: 4506 Rating: (836)
|
Hello, It can be used for two CPUs or more.
|
Ayman Elotaify |
|
This contribution was helpful to3 thankful Users |
7/1/2013 7:05 AM | |
Joined: 11/8/2011 Last visit: 4/12/2024 Posts: 387 Rating: (43) |
HI profibus communication network in between 3 PLC315-2dp |
7/1/2013 7:53 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
All of them are Masters? If they are - you can not make "real simulation"! |
7/1/2013 8:34 AM | |
Posts: 153 Rating: (2) |
Check these links also, you may find some thing useful to you...:: /tf/WW/en/Posts/92117 http://support.automation.siemens.com/WW/view/en/36068796 https://support.automation.siemens.com/WW/llisapi.dll/csfetch/36068796/S7_PLCSIM_V54_SP3.zip |
Follow us on