4/18/2017 5:16 AM | |
Posts: 1 Rating: (0) |
Dear All, Our user have existing configuration as follow 1. Redundant PLC Process and Safety using 414-4H (Process : 2 CPU, Safety : 2 CPU) 2. There are 4 standalone HMIs (WinCC v6.0 SP4, OS : Windows XP SP2) as follow a. HMI 1 and 2 are monitoring internal process b. HMI 3 and 4 are monitoring export metering process User is planning to upgrade : 1. Redundant PLC Process and safety from 414-4H to 414-5H 2. Upgrade only HMI 4 3. Combine two applications of WinCC so each HMI has identical application Please advise the SOP to upgrade the PLC and HMI. regards, Jerry AttachmentSystem Architecture Drawing.pdf (30 Downloads) |