12/9/2016 8:58 AM | |
Posts: 11 Rating: (4) |
The situation is as follows. - I uninstalled WinCC 7.4 - Installed WinCC 7.3 Update 1 - Opened WinCC Explorer and created a new project - It stops at a certain point with error message:"A basic application could not be started, please check your software license" Afterwards the message project could not be created appears. I can see it stops right after loading the Tag management section. As you can see WinCC Explorer runs in Licensed mode (see attachment). Also Windows is activated. The attached PMDiagnose lists error 2016-12-09 15:28:50.915 PM(2768-5484) CCImpersonate::CCImpersonate failed for ImpersonateLoggedOnUser with error 6: The handle is invalid. 2016-12-09 15:28:51.352 PM(1000-6064) Parameter {1} ignored Does anyone knows what to do? I must say i WinCC 7.3 Update 1 on a Windows 10 system. I have succesfully installed and working versions of WinCC 7.3 Update 1 on other Windows 10 machines. So i am not sure running Windows 10 is the reason of this failure.
AttachmentPMDiagnose.zip (596 Downloads) |
12/29/2016 2:05 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hello, Windows 7.3 isn't released for Windows 10; the two may or may not work together, but there is no guarantee, so it's quite possible that your choice of OS is the reason for your problem.. You'll find out more with the Compatibility Tool. Some information is also in this thread: https://support.industry.siemens.com/tf/ww/en/posts/wincc-7-3-compatible-with-windows-xp/117587/?page=0&pageSize=10 Best regards |
Grundkurs/Systemkurs WinCC V7: |
|
7/10/2017 5:26 PM | |
Posts: 22 Rating: (0) |
was there a resolution to this? I am now experiencing this issue with WinCC 7.3 and Server 2012 after a re-installation. |
2/22/2018 5:20 PM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating: (12) |
Same problem here. Windows 10, WinCC 7.4 SP1. DId anyone find a solution? |
3/1/2018 6:01 AM | |
Posts: 5 Rating: (0) |
Hi Priyanka, Even i am facing the same issue from last two days,please let me know if you have fixed this issue.It will be great help for me.Thanks in advance. |
Follow us on