6/27/2013 1:08 AM | |
Joined: 9/27/2006 Last visit: 9/19/2025 Posts: 12415 Rating:
|
Hello desmul; In the following link you will find first a link to our friend Hamid's S7 code (in STL) to do this conversion in the PLC, and further the same code in LAD. Convert to S5TIME Umencho also provides in the same discussionadocument explaining the structure of the BCD-coded value of as S5Time variable, which might help you design yourscript. Is it absolutely required to do this script in the HMI, when you have working code to do it in the PLC? Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on