2/14/2020 4:19 PM | |
Joined: 1/23/2020 Last visit: 3/7/2024 Posts: 9 Rating:
|
Hi All, We have S7300 CPU 315-2 DP & IFix scada, Intermittently there is communication drop between PLC and SCADA. After seeing values not being displayed on scada (this happens only for few seconds) when we check the PLC it is always in run. Below is the diagnostic buffer from PLC which is confusing as it says the PLC was in stop mode for some time. Can someone please help in identifying the problem. Diagnostic buffer of module CPU 315-2 DP [snip]
AttachmentDiagnostic_buffer.txt (423 Downloads) |
Last edited by: Simatic_Fann at: 02/14/2020 16:21:38Last edited by: Jen_Moderator at: 02/17/2020 10:59:22Added Diagnostic Buffer as a txt file. |
|
Follow us on