(0)| 4/17/2020 6:09 PM | |
|
Joined: 6/6/2017 Last visit: 12/1/2025 Posts: 44 Rating:
|
Hi, I have a similar problem, but I believe is a little bit complicate. I have a LOGO! 8 FS4 but unfortunately the display is damaged and I can't see any thing but some pixels but all the rest is working fine. I want to use the scroll buttons to set functions in the program, I already programmed the actions in the software using the C1 to C4 arrows, but is doing nothing and I can't see why because the display is damaged. So, I have a lot o questions for this situation: 1°: I tried to do the firmware update to see if the screen back to normal because if the pixels are working maybe is not a hardware problem, but again I couldn't see what happened but the firmware stays the same that I confirmed by the LOGO! soft Comfort. This is the first question: The firmware can solve the display problem? 2°: How can I use the arrows keys to act as a input? I can't see the display, so I need to know exactly what button sequence I need to press to allow the operation. 3°: I know that is a lot of work but can somebody post all LOGO! 8 FS4 screens like a flowchart to I know what I'm doing in this LOGO!? Thanks so much ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/20/2020 08:55:41New subject after splitting |
|
Follow us on