6/8/2023 9:19 AM | |
Joined: 7/19/2022 Last visit: 9/25/2024 Posts: 384 Rating: (62) |
Hello m.shakshoki1, There is no possibility to open/edit a panel project in the TIA Portal. .brf files are not editable. This is because when you load the project in a panel, a build of the project is loaded in the panel and not the program itself. |
If this Information really helps, you could use the Rate function |
|
6/9/2023 10:47 PM | |
Joined: 10/22/2011 Last visit: 9/25/2024 Posts: 43 Rating: (0) |
hello thanks for your interest i could open the project in RT simulation but still i need open edit best regards |
Follow us on