8/17/2023 7:52 AM | |
Joined: 2/17/2020 Last visit: 10/18/2024 Posts: 1090 Rating: (197) |
Hi, Maybe you could share pictures of what should and doesn't show when doing the restore in the new Comfort Panel? Really, the backup should include all the graphics and program objects/elements, since the only exclusions that can be made when doing the backup are related to recipes and user administration. However, if the downloaded program has an inconsistent build, I'm afraid you'll need the original OEM program to remove the IM folder, rebuild all and download it again. |
A rating will be well appreciated. |
|
8/23/2023 2:58 AM | |
Joined: 1/21/2021 Last visit: 11/6/2023 Posts: 3 Rating: (0) |
This is the original display. |
8/23/2023 2:58 AM | |
Joined: 1/21/2021 Last visit: 11/6/2023 Posts: 3 Rating: (0) |
And new HMI with missing graphic |
Follow us on