8/22/2023 4:03 PM | |
Joined: 5/30/2022 Last visit: 7/17/2024 Posts: 553 Rating:
|
Hi AutoGen_1894858, To make the backup to the TP 177B 6" DP panel you can use the following cables:
|
If this information really helps, you could use the Rate function. |
|
8/23/2023 3:07 PM | |
Joined: 8/8/2023 Last visit: 7/11/2024 Posts: 2 Rating:
|
thank for your help, I have another question, i just found out when turn on HMI, in screen display model TP177A but model in the back is TP 177B 6" DP; I open inside HMI and see only 1 port MPI/PROFIBUS. I search manual TP 177B , it has port MPI; usb and SD card. I'm really confused, how can i determine which model it is? |
Follow us on