10/20/2023 2:22 PM | |
Joined: 5/6/2022 Last visit: 8/7/2024 Posts: 439 Rating: (86) |
Hi Clem_123456789, To have some more information, could you give us more information so we can help you? What HMI panels are you using Basic/Comfort/Unified? What image version do you have installed? What exact version of TIA Portal are you working with and with which you created the project? On the other hand, I would like to tell you that in principle to connect remotely from one panel to another there is only the Sm@rt Server option. Additionally, I am sharing a FAQ where you will find information about this remote access in case it is helpful: In the Unified Comfort panel you aso have the option of Collaboration. I share you another link with this information: "SIMATIC HMI WinCC Unified Engineering V18: Basics" Best regards!!
|
Last edited by: ElonksuM_SN_BN at: 10/20/2023 14:28:39If this Information really helps, you could use the Rate function |
|
10/25/2023 3:05 PM | |
Joined: 3/22/2023 Last visit: 5/31/2024 Posts: 14 Rating: (0) |
Perfect, thank you very much ! I didn't know about this option |
Follow us on