3/28/2024 2:42 PM | |
Joined: 9/27/2022 Last visit: 4/18/2024 Posts: 2 Rating: (0) |
Hello All, I'm having trouble to open and upload the programme for S7-400 with a TIA portal V16. I have an error message not supported 0030:000001 " the following software are not available and need to be installed before you continue: STEP 7 proffessional" please can anyone help, I do not know which software was used to program the S7-400 . the error related to the version of software. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/28/2024 14:54:36New subject after splitting |
|
3/28/2024 3:00 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349)
|
Screenshot of the "following software" dialog box would be helpful. Or, simply read what it says and install that software (or install any required updates and/or service packs .. and updates).
|
science guy |
|
4/1/2024 2:53 AM | |
Joined: 2/28/2023 Last visit: 4/22/2024 Posts: 32 Rating: (1) |
Hi Sharing the list of the following software needed to be installed? However the error message could be as a result of STEP7 Professional non availability or needs to be installed before proceeding, which is related to version of software installed. To resolve 1. Check effective installation of STEP7 professional: Do you have STEP7 Professional installed? 2. Check compatibility: Verify STEP7 professional version compatibility with TIA portal v16 3. Update TIA portal: Ensure portal V16 is up to date, check for update and apply Delivery release TIA Portal V16 - ID: 109771626 - Industry Support Siemens 4. Don't forget to restart TIA portal after every installation or update ------------------------------------------------------------------------------------------------------If it is resourceful then rate it. However you are not obligated. |
Last edited by: Deyoung at: 04/01/2024 02:54:14Last edited by: Deyoung at: 04/01/2024 03:27:36Cheers. |
|
Follow us on