1/25/2024 7:28 PM | |
Joined: 7/26/2022 Last visit: 5/4/2024 Posts: 8 Rating: (0) |
Hello , we have a H-System with one cp443-1 (1EX11) in each rack and one Os server. we have a problem with importing XDB file into OS Server when we have one CP1613 A2 everything's is fine and AS can communicate with Os server but when we add another CP1613 A2 on os server for redundancy in plant bus we got this error in station configuration as below : ***The MAC address for the configured component is already being used on the target computer by another module, please assign a diffrent MAC address!*** we changed mac address but the problem still exist The MAC address related to two CP1613 A2 are correctly configured in Os server configuration and also in netpro we created fault tolerant connection between AS and OS ------------------------------------------------------------------------------------------ |
Last edited by: Engkourosh at: 01/25/2024 19:52:09Last edited by: Jen_Moderator at: 01/26/2024 11:59:36New subject after splitting Last edited by: Engkourosh at: 01/26/2024 16:15:46 |
|
2/1/2024 6:48 AM | |
Joined: 7/26/2022 Last visit: 5/4/2024 Posts: 8 Rating: (0) |
Hello Murof thanks for reply I also unistalled the cp driver and removed the simatic net and reinstall again but the problem still exist Attached, please find the file below AttachmentCP1613 configuration.zip (167 Downloads) |
2/1/2024 8:52 PM | |
Joined: 7/26/2022 Last visit: 5/4/2024 Posts: 8 Rating: (0) |
has anyone run into the same problem? |
Follow us on