9/14/2024 7:29 AM | |
Joined: 3/19/2019 Last visit: 9/23/2024 Posts: 104 Rating: (0) |
Hi dchartier, I am having the network issue with S7410E PLC with all the IM55-6 modules, I added diagnostics buffer here. I changed the update time for all the IM modules from automatic to 64ms. but still issue not solved. Kindly help us to solve this issue. Diagnostic buffer: Event 26 of 3200: Event ID 16# 72A5 PROFINET IO: return of redundancy at station Address of the affected station: Input address: 16351 IO system ID: 102 Station number: 4 Log. base address of the IO controller: 16363 Requested OB: I/O redundancy error OB (OB70) Priority class: 24 Outgoing event 10:40:50.878 AM 09/14/2024 (Coding: 16# 72A5 1846 C454 3FEB 3FDF 9004) Event 27 of 3200: Event ID 16# 38CC PROFINET IO: station return but disrupted/in maintenance Address of the station involved: Input address: 16339 IO system ID: 100 Station number: 7 Log. base address of the IO controller: 16383 Requested OB: Rack failure OB (OB86) Priority class: 25 External error, Outgoing event 10:40:48.992 AM 09/14/2024 (Coding: 16# 38CC 1956 C454 3FFF 3FD3 8007
------------------------------------------------------------------------------------------ AttachmentCPU Diagnostic Buffer 14092024.pdf (342 Downloads) |
Last edited by: Moderator_Lan at: 09/16/2024 11:08:10New subject after splitting "If you want the answer - ask the question" |
|
Follow us on