10/14/2024 10:22 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi, For more information about this topic, see the following manual at page 39: PCS 7 Software update without utilization of new functions for SIMATIC PCS 7 V9.1 SP1 You probably are using an old library which is not installed on the V9 ES. Maybe it works if you compile the program without module drivers (remove checkmark: Generate module drivers during CFC Compile). You have to do that each time you start a compile. Otherwise, you need to install the old libraries used in your project. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on