7/8/2009 8:34 AM | |
Posts: 6 Rating: (0) |
Is it possible to program a kind of Astro function with LOGO. |
7/8/2009 11:45 AM | |
Posts: 173 Rating: (95) |
(This is me looking at the sun!) Hi Astro-followers! There have been a couple of 'cool' short programs on the German one to determine when the sun rises or sets. Check out Unlike another rmanufacturer that says that they have a solar tracking function library built into their unit (that takes up almost all the programming space! no space left for a decent program!), the LOGO! does not have complex internal mathematical calculation capabilities - it knows ON/OFF, integer values, counters and timers. Are you needing a function that turns ON when it is officially SUNRISE and OFF when it is officially SUNSET? How accurate does it have to be - in the German forum, the one user says that it only needs to be about 20 minutes accurate. |
7/8/2009 11:53 AM | |
Posts: 153 Rating: (15) |
Hi, one can try to use the LOGO with timers which contain the Astro function via EIB. |
7/8/2009 3:04 PM | |
Posts: 6 Rating: (0) |
Thanks everyone Found it on the german site!!!! . 20 min preciscion is ok. only for garden lightning. Lykou |
Follow us on