10/6/2016 10:42 AM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
We provide an SD-Card Example Image. If you want to create your own image, you can do this as well. Required for this is a Linux based building environment. The following builds have been successfully tested on Debian 8 and OpenSuse 13.2, but other recent distros are expected to work as well. There are two build instructions (README.md) to do so on GitHub (https://github.com/siemens/meta-iot2000): At first there is the “meta-iot2000-bsp”, which is the official board support package. It allows building standard Yocto images which will contain the required kernel, configurations and tools and will emit a bootable SD card image. Based on this there is the “meta-iot2000-example”. This Yocto layer builds on top of “meta-iot2000-bsp”, providing an exemplary image with additional tools and services to exploit features of the IOT2000 conveniently. This layer shall only be considered as a starting point for own developments. It is not configured to provide product-grade maturity and security. If you follow the instruction for building the “meta-iot2000-example” layer, you will get exactly the SD-Card Example Image provided by us. |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/26/2017 8:58 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
FYI: Santiago's report is now tracked at https://github.com/siemens/meta-iot2000/issues/51. |
7/26/2017 11:56 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
Please see https://support.industry.siemens.com/tf/ww/en/posts/building-latest-sd-card-image-simplified-process-available/171736/?page=0&pageSize=10 for an update on & simplification of the build procedure. |
3/27/2018 1:44 PM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, there is a branch on our github page. Have a look at branch jan/rocko. There are no security aspects but username and password as I know. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
4/19/2018 9:18 AM | |
Joined: 2/28/2018 Last visit: 10/19/2023 Posts: 9 Rating: (0) |
is the description on: https://www.dmcinfo.com/latest-thinking/blog/id/9395/creating-a-linux-image-for-the-siemens-iot2000-series just outdated(and due to this more complex)? Or is is wrong? Because I have the same error and then I tried to use "kas", but that failed, too. |
Follow us on