11/18/2024 11:24 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, No, you won't need to use the OpenAut/CloseAut signals. You can use it to directly sent the valve to open/close position and check the feedback signals FbkOpen and FbkClose. Using the MV_Ext is just fine. The VlvAnL can also be used to control an auxilliary valve connected to the analog valve. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on