(0)| 5/15/2024 9:19 AM | |
|
Joined: 5/2/2024 Last visit: 5/26/2025 Posts: 1 Rating:
|
Hi everyone, in the simatic shell , server and client can not see each other .. Please help |
| 5/17/2024 2:06 PM | |
|
Joined: 2/17/2020 Last visit: 12/26/2025 Posts: 1251 Rating:
|
Hi, Make sure you have configured the hosts and lmhosts files for name resolution between PCs: What are the requirements for operating SIMATIC WinCC in a Windows network? |
|
A rating will be well appreciated. |
|
| 6/3/2025 2:32 PM | |
|
Joined: 6/3/2025 Last visit: 6/10/2025 Posts: 1 Rating:
|
Hi, I have the same problem with the first commentator; while trying to set a server client configuration in WinCC Pro V14 SP1 UP10, I linked two pcs with a standard ethernet cable, connected them with TCP/IP v4 with IP Addresses and Subnet options filled up. The problem here is that when I go to “This PC→Simatic Shell” I only find my computer under “Simatic Shell” (I did update and choose a network adapter option under Simatic Shell→ settings).
I followed the video tutorial https://youtu.be/KDSVQJ0VOyM?t=664 . I did all the steps until 11:04, and the only thing is that I used an actual second pc instead of a virtual machine.
Also, If I need an update regarding my WinCC and TIA Portal versions, how can I convert a v14 project to the new version suggested.
Thank you in advance for Replying. |
Last edited by: Moderator_Lan at: 06/03/2025 14:37:50Video embedded |
|
| 6/4/2025 1:54 PM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello first of all you should check every single setting in this FAQ on both sysems: https://support.industry.siemens.com/cs/de/en/view/108464289 if you cannot see each other in SIMATIC Shell you can also try to use each other as Multicast Proxy, this helped me also a few times Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
|
|
Follow us on