(0)| 11/3/2021 9:02 AM | |
|
Posts: 3 Rating:
|
Dear Sirs PC, PLC (S7-200 SMART CPU ST-60 and HMI are individually connected through Ethernet and PLC CONNECTION is also visible on access to on line devices with IP address as: 192.168.2.1 for PLC and 192.168.2 for HMI. Neither HMI and PLC data exchange nor Rx Tx led are are blinking. On PLC programme status, PLC information are OK HMI is programmed with TIA 13 and PLC with V2.5 version software. Fault monitoring bit in PLC SM4.3 AND SM5.0 shows no Error. ST60 is configure with a few I/O modules and in test these are missing. Kindly guide as we are not able to move with project Dr D S Tomar ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/03/2021 11:06:07New subject after splitting |
|
Follow us on