5/13/2024 2:30 PM | |
Joined: 4/21/2019 Last visit: 5/13/2024 Posts: 9 Rating: (0) |
Hello everybody! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/14/2024 04:41:30New subject after splitting. Text formatting optimized. |
|
5/14/2024 4:04 AM | |
Joined: 3/30/2020 Last visit: 6/13/2024 Posts: 4596 Rating: (954)
|
The message says you have updated a part of TIA Portal to V19 Update 2 but did not update all the components of the software. For example you could have Wincc Unified at V19.0.0.2 but Step7 and Wincc Advanced is not on V19.0.0.2. Consider installing the update for Step7 / Wincc first. For precise information you can contact Siemens using the "Support Request" link. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
5/14/2024 5:45 AM | |
Joined: 1/21/2013 Last visit: 6/15/2024 Posts: 2887 Rating: (462)
|
Hi Lhm250, Do you have Startdrive V19 installed? This is probably the cause of the problem. As Startdrive is delivered in a cumulative package, installing Startdrive V19 SP1 will update the TIA Portal Framework to Update 2. This means that STEP 7 and WinCC also need Update 2. This information can be found in the sales and delivery release for SINAMICS Startdrive V19 SP1. When using Startdrive as optional package for STEP 7, the installation of STEP 7 V19 Update 2 (109925643) is a prerequisite for Startdrive V19 SP1. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on