3/22/2022 2:47 PM | |
Joined: 2/2/2021 Last visit: 10/8/2024 Posts: 12 Rating: (3) |
Hello, With W10 updated (2022/03/22) and with the lasted version of Tia Administrator V1.0 + SP4 + Upd2. The access to the server with chrome and Edge is not working with the following message: ERR_SSL_SERVER_CERT_BAD_FORMAT But it works with Internet Explorer Is there a specific setting to be done with Edge to allow the certificate? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/23/2022 09:44:33New subject after splitting |
|
7/21/2022 7:07 PM | |
Joined: 11/25/2011 Last visit: 10/13/2024 Posts: 5 Rating: (0) |
Have been dealing with the same problem.... Thordur |
1/9/2023 1:05 PM | |
Joined: 2/2/2021 Last visit: 10/8/2024 Posts: 12 Rating: (3) |
Hello, I'm back to my topic, I have also the problem with the Tia ADMIN V2 with Edge application. My PC uses a Windows 10 pro updated with the latest version. I found this topic the help me to solve the issue with a Short-term remedy by using FireFox. It seems that the problem is linked to the last version of Windows and also the regional parameter. Best regards.
|
Last edited by: Jen_Moderator at: 01/10/2023 07:06:54Link optimized. |
|
This contribution was helpful to2 thankful Users |
Follow us on