5/10/2024 7:41 AM | |
Joined: 3/30/2020 Last visit: 5/25/2024 Posts: 4537 Rating: (946)
|
One step backwards please: Why do you wish to export to XML? One option is to use the Export-Import add-in listed here: The Openness Scripter is a good idea when you have Step7 versions prior to V17. You can get the installation: [LINK: Tool for easier use of the TIA Portal Openness interface (Openness Scripter)]. As you noted, some application code has already been created and published on the forum. Depending on your actual use case, it may be better to export coding via the library functionality. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on