10/8/2024 8:11 PM | |
Joined: 3/4/2022 Last visit: 10/10/2024 Posts: 3 Rating: (0) |
For a few days now I have been struggling with a problem that occurs when adding a new device. When I click ""Add new device" in the project, the program freezes for a dozen of seconds and then displays the error screen that I have attached. I will add that I have already uninstalled everything from the system that has V17 in the name twice and then reinstalled it. I also tried opening it as an administrator. Generally, I suspect that when I was adding Unified panels in the past, some package was installed that had the name "TIA Portal V17 Prof Ed French". From the stacktrace I can see that it is some kind of language problem. I do not know where this "French edition" came from in the system since I installed the normal V17 with the partner package. Please help because I have no more ideas. I am attaching the StackTrace.
AttachmentStackTrace.txt (7 Downloads) |
Last edited by: Moderator_Lan at: 10/09/2024 07:37:57Text formatting optimized/ Code attached Last edited by: Moderator_Lan at: 10/09/2024 07:38:42Text formatting optimized/ Code attached |
|
Follow us on