12/20/2023 5:28 PM | |
Joined: 10/14/2017 Last visit: 5/28/2024 Posts: 26 Rating:
|
Hello, I have a RF240R RFID Reader with IO-Link. This device is connected to a external vendor profinet unit from Festo. This unit is already connect and provide the port and the 32 bytes of in/out. And using the template below i was already able to check presence of a rfid tag: https://support.industry.siemens.com/cs/pt/en/view/73565887 However when i trigger read or write functions i never get feedback from the functions. (Inside the FB is stuck inside Switch antenna on). Question: Should i really use this template or this is just to use on siemens io-link ports? Do i need to configure something with the PCT Tool? What should i put on the port address input of the FB? Is there another way to do this? Thanks in advance. |
Last edited by: Jen_Moderator at: 12/21/2023 10:23:37Link optimized. |
|
6/27/2024 9:36 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8202 Rating:
|
New question published by AutoGen_945108 is split to a separate thread with the subject RF210R IO-link from External Vendor. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on