1/29/2024 11:08 AM | |
Joined: 2/13/2019 Last visit: 6/6/2024 Posts: 6 Rating:
|
Hi all, In Simit 11.0, we've set up a OPC UA client coupling to an external server. This coupling is set up to be in time slice 1, having set up a update rate of 250ms (time slice 1 =250ms) and a multiplier per signal of 1. This is such as the operation manual describes it in Section 2.9.2: I have in total 12 analog signals. The OPC UA server updates the these quite frequently (at least faster than 10x per second). When I'm monitoring these with a generic OPC UA client viewer (such as softing opc ua client), I can refresh/read them as fast as I can press my mouse button. Now when I run my simulation in simit, the update rate within simit is more like once per 2 seconds, which is way too slow. I've reduced and increased the time slice size, but this also doesn't seem to increase my update rate. How would I increase my update rate? |
Last edited by: Jen_Moderator at: 01/30/2024 08:10:34Last edited by: Jen_Moderator at: 01/30/2024 08:11:01*Link optimized. |
|
1/29/2024 12:23 PM | |
Joined: 1/11/2019 Last visit: 6/28/2024 Posts: 726 Rating:
|
Hello Kweenie, Could please share the external server details? |
Follow us on