5/14/2024 7:28 PM | |
Joined: 1/15/2019 Last visit: 6/4/2024 Posts: 1 Rating:
|
Now I have the same problem: on the G120C frequency driver (FW: V4.7 SP13 HF4) both LEDs light up red: RDY and BF.When BOP-2 is set, it displays: CU BUSY (and) SEARCH 1200,,4200,,9200, and these displays are repeated, changing constantly.I tried to connect with USB or Profinet without success. is it possible to restore factory settings with a 4mb memory card? If this is a firmware issue, is it possible to change or refresh FW with the 4MB memory card as that's all I have right now? Anyone who knows or has any suggestions, ASAP. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/15/2024 08:59:31New subject after splitting |
|
Follow us on