8/12/2024 2:45 AM | |
Joined: 7/21/2022 Last visit: 8/19/2024 Posts: 11 Rating: (0) |
Hello, I have issue for TP1200 HMI. I programming PLC program in TIA prtal and HMI TP1200 also. It was no problem. But recetly turn off whole machine in plant. And HMI have some problem when turn on again. You can see attached photo. (1) Now HMI do not displayed data value. (####) But all button is working. And communication also no issue. So i try to download to HMI. But it is not working. (2) So i do not understand he is doing like this, and want to know solution. AttachmentTP1200 issue.pdf (259 Downloads) |
8/12/2024 9:45 AM | |
Joined: 8/6/2018 Last visit: 10/18/2024 Posts: 292 Rating: (40) |
Hello, Have you tried factory resetting the panel and reloading the project? Thanks you |
8/12/2024 10:03 AM | |
Joined: 7/21/2022 Last visit: 8/19/2024 Posts: 11 Rating: (0) |
Now this TP1200 not working for factory resseting also. |
9/6/2024 9:20 AM | |
Joined: 8/3/2009 Last visit: 10/18/2024 Posts: 13982 Rating: (1760)
|
Hello JK.Seo here is a manual how to do a reset to factory settings: https://support.industry.siemens.com/cs/ww/en/view/19701610 Check if this works, if not then it would also be a good idea to contact the Siemens Technical Support for further help. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on