7/28/2015 5:40 PM | |
Posts: 5225 Rating: (1192) |
Andy, The HSC (high speed counter) can be used as a counter or to give "frequency" feedback. It is the frequency feedback that I think you need. the HSC in frequency mode has the potential of saving you from a lot of coding. PLEASE do make note of what our friend huggy_d1 has said. many people are having problems with this. I hope to put your attention to a file called "Quick & Dirty_HSC for frequency indicator.pdf". This file can be seen in two threads. Please read through the PDF first and then work through both of the threads.. taking from it what you need. [LINK1] [LINK2] If any questions.. do not hesitate to ask. Greetings. |
Follow us on