12/3/2020 7:55 PM | |
Joined: 9/23/2005 Last visit: 9/9/2024 Posts: 4347 Rating: (1442)
|
“Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: Alarm messages are an important tool for operation diagnose of process and system events. The possibility to generate messages directly from the controller's blocks reduces the HMI configuration time. In this sample, a controller's user program generates message on a HMI, calling the Program_alarm block. Configuration main steps: On Controller side:
TIPs:
On HMI side:
Note: as comparation proposes, the sample project has both analog alarm and PLC alarm. Project: Archived program, compressed (zip) AttachmentProgramAlarm.zip (1070 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
Follow us on