10/5/2016 5:01 PM | |
Joined: 5/31/2016 Last visit: 8/9/2022 Posts: 20 Rating: (0) |
This is the RS-485 extension module, it has mounted x1 port of pac4200. Actually, configuration I made at Powerconfig side is very simple. When I broadcasted devices, it founded automatically with properties which had made inside of it. I put screenshots of it, I guess it is much more easy to tell. pac4200 and pac3100 . This configuration works perfectly. I agree with you, also thinking about there is something wrong while data conversion. But at this topic ExigoMCL said that;
And its Scheider device, I am trying same thing with Siemens own device. So it seems meaningless. With best regards.. |
Last edited by: 21321 at: 10/5/2016 5:02:01 PM |
|
10/6/2016 2:30 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, also this link can be helpful, especially about RTU over TCP: http://www.simplymodbus.ca/TCP.htm |
With best regards... |
|
Follow us on