9/17/2023 7:31 AM | |
Joined: 7/29/2021 Last visit: 10/12/2023 Posts: 2 Rating: (0) |
We are designing and manufacturing a lathe machine with 7 axis and spindle total 8 axis with CNC SOFTWARE 26x, TURNING, CF WITH LICENSE 6FC5834-1GY40-6YA0
we need to add third axis S2 as slave 2 In speed control mode with Master Z axis option two Z and s1 motor on Master slave and Z and s2 motor as Gantry axes as speed control we need to confirm the coupling three axis in Siemens 828d before placing order with Siemens . AttachmentSIEMENS MOTOR DETAILS (2).pdf (301 Downloads) |
Follow us on