6/4/2010 5:27 PM | |||||
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Hi Please check the attachment for more detail.I am using STEP7 V5.3 and downloaded new HSP file from this link:
AttachmentHD.zip (356 Downloads) |
||||
11/18/2014 4:54 PM | |
Joined: 3/7/2011 Last visit: 7/29/2024 Posts: 7 Rating: (0) |
It seam I have the same problem. I neded to upload a PLC configuration and soft from an excisting CPU315-2 pn/dp v2.6. I could upload the hardware exept fore the CPU. The problem is that the V2.6 is not i my hardware catalogue. I updated the catalogue but the v2.6 of the CPU is not available in the download. I use the s7 V5.5 SP4. The CPU is the 6ES7 315-2EH13-0AB0. where can I find the file fore my HW S7 HW catalogue?
|
Last edited by: VGK at: 11/18/2014 4:55 PM |
|
11/18/2014 5:40 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
If you have already upgraded your hardware catalog? HW Config> Tools> install hardware updates. Follow the instructions. |
11/19/2014 9:19 AM | |
Joined: 3/7/2011 Last visit: 7/29/2024 Posts: 7 Rating: (0) |
tryed it. The cpu is not in the download list and not in the install list. The higest version is the cpu31x-2dp/pn v2.5. I need the v2.6. If sommeone has this version in his library you may always send it to me. |
11/19/2014 9:55 AM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
I have also the Version V5.5 SP4 and the 6ES7 315-2EH13-0AB0 V2.6 is into the hw-catalog. |
Last edited by: 190B at: 11/19/2014 9:56 AM |
|
11/19/2014 10:36 AM | |
Joined: 3/7/2011 Last visit: 7/29/2024 Posts: 7 Rating: (0) |
I have the same step7 soft version, I updated the HW catalogue but it's diffrent from yours. I did install the step7 on a neuw pc windows 7 64 bit. Do you have sommething els? |
Follow us on