2/6/2018 1:04 PM | |
Joined: 10/26/2011 Last visit: 8/30/2024 Posts: 762 Rating:
|
CPU 300 are not completely integrated in PCS 7. You have to integrate these CPUs with the Industry Library. With it you get new blocks, generate for the connection between CPU300 and PCS 7 / OS Runtime. The faceplate are in the APL loo&feel, but not the same. How you integrate CPU 300 with the Industry Library is described in the application example "Integration of Comfort Panels, Operator Panels and S7-300 Package Units in SIMATIC PCS 7 with PCS 7 Industry Library" Further information to Industry Library Manual PCS 7 Overview Cpmpatibility of IL with PCS 7 |
Last edited by: Thunderstorm at: 2/6/2018 1:08:23 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to
1 thankful Users |
2/6/2018 1:07 PM | |
Joined: 10/26/2011 Last visit: 8/30/2024 Posts: 762 Rating:
|
Please see also the post: It shows, which hardware profile you have to select. |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
1 thankful Users |
2/8/2018 7:45 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hello Din Islam, to your questions:
With regards |
This contribution was helpful to
1 thankful Users |
Follow us on