5/26/2014 9:47 PM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating:
|
Hello xuanphu, Look on the FAQ, How do you create dynamic text lists? its same you are looking for ???????? |
Ammy |
|
This contribution was helpful to
1 thankful Users |
5/27/2014 5:41 AM | |
Posts: 146 Rating:
|
This is my example ..Please change SCADA example.zip to SCADA example.rar...then unpacking... Please ..check it for me ! Thank you very much ! AttachmentSCADA example.zip (136 Downloads) |
5/27/2014 9:10 AM | |
Posts: 146 Rating:
|
I'm using WF 2008 SP3 ...V1.4.0.0_16.0.16 Build I downloaded then unpacking and run...It's normal ...Please check it for me again ! Thank you very much ! |
5/28/2014 7:35 AM | |
Posts: 146 Rating:
|
Anyone ..Please help me ..till now...I still couldn't do it....Not hard but also not easy to do... THank you ! |
5/28/2014 10:10 AM | |
Posts: 146 Rating:
|
Thank you very much for reply ! Now I send to you my file after saving as winccflexible sp2 format .......Please remeber changer extention name from Zip ---> Rar.... Thank you very much ! AttachmentScada example 2.zip (156 Downloads) |
5/28/2014 1:56 PM | |
Joined: 5/28/2008 Last visit: 8/31/2024 Posts: 4515 Rating:
|
Hello Please have a look on the attached project. And please change extension from *.ZIP to *.RAR I have created another symbolic IO field for you and it write in MW50. Then in code, you will prepare only one network If MW 50 = 0 => stop the motor If MW 50 = 1 => start the motor Hope this helps.
Attachmentsupport_01.ZIP (133 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
5/31/2014 5:42 PM | |
Posts: 378 Rating:
|
Hello, For the sake of saving resources, if you have two operations (start & stop), it is better to use bool tag (DB1.DBX4.0 = 0 > stop, DB1.DBX4.0 = 1 > start). At your plc: [code]A DB1.DBX 4.0 = Q 4.0[/code] Have a look at my attached example (rename to .RAR) Rgs AttachmentScada example 3.zip (167 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on