6/12/2006 8:57 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Dear all, I think that this is possible. There is something written about it in the Scalance W Client manual: http://support.automation.siemens.com/WW/view/en/19386812(page 126 and further). This is only supported by the Scalance W746, W747 and the W788-1, W788-2. If I am right is what you want to do the following: 192.168.10.1== port 1000| | 192.168.20.3192.168.20.10 192.168.10.2== ========= ========= port 1001 ||Scalance||Scalance | |===| Client | ))) (((| AP |=NETWORK | | | | | 192.168.10.3== ========= ========= port 1002 | | 192.168.10.4== port 1003 And if I understand the manual correct then it's possible [:D] with the following settings: In the client it is possible tofill in the IP-addresses of the wired network devices and nodes on the client side. When you fill them in you have to couple an internal port to every IP-address. This port is necessary because if you want to reach the node from the "outside". So if you are connected on the NETWORK-side with a PC (192.168.20.5) in the abovecreated example and you want to reach one of the nodes on the wired-side of the client you have to use the following IP-address 192.168.20.3/1000 So I hope that my explanation is clear to you. [:D] Best regards, INS |
Last edited by: INS at: 6/12/2006 9:09 PMMaking a drawing this way is not easy, <img src="/forum/en/skins/emoticons/emotion-5.gif" alt="blink" /> Last edited by: INS at: 6/12/2006 9:00 PMLast edited by: INS at: 6/12/2006 9:00 PMBest regards, |
|
6/19/2006 8:27 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
HiLate, If you mean with your post the communicaion from the client-side towards the NETWORK-side then this will be possible. The best explanation from this is made in the Scalance S manual in chapter 5.7. http://support.automation.siemens.com/WW/view/en/21718449 Best regards, INS |
Best regards, |
|
6/20/2006 9:59 AM | |
Posts: 5822 Rating: (412)
|
Hi to you both, well, this is very clear... for SCALANCE S but where do you find this in SCALANCE W? |
6/20/2006 7:15 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hello J_Bell, INS |
Best regards, |
|
Follow us on