2/23/2024 1:26 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi, If permit is 1, it is allowed to leave the neutral position of the block. For a motor, it means it can be started. If the motor for example is already running, permit has no further use. If permit is 0, you cannot start the motor. |
If I could help you, you can use the RATE button. Thank you. |
|
2/28/2024 7:43 AM | |
Joined: 9/4/2020 Last visit: 9/17/2024 Posts: 6 Rating: (0) |
Thank for reply. But i didn't find permitsafepos bit jn my motl block |
2/28/2024 3:07 PM | |
Joined: 1/11/2019 Last visit: 10/7/2024 Posts: 764 Rating: (151)
|
Yes! You are right.. Its not working in PCS7 V9.1 Kindly update the PCS7 to recent release PCS7 V9.1+SP2 UC03 |
Last edited by: Techno_Taru at: 02/28/2024 15:08:29 |
|
Follow us on